MITSUBISHI ELECTRIC endringer til det bedre

In this case study...

  • Mobile full-scale A320/B737 aircraft fire simulator,
  • 28 realistic fire simulation scenarios for emergency training,
  • Real-time performance monitoring and assessment,
  • Advanced automation for safe and reliable operation,
  • Customisable training environments for airport-specific requirement.

Airport firefighting crews operate in highly complex environments where every decision matters. Yet creating realistic training conditions for rare but critical incidents—such as aircraft fires or fuel spills—can be challenging. To close this gap, Fire GO GmbH developed a mobile aircraft fire simulation system that utilizes Mitsubishi Electric’s advanced automation technology, enabling airports to deliver scenario-based training directly on-site.

The challenge: from unpredictable to prepared

Airport firefighters must be ready to respond immediately to a wide range of emergencies, from cockpit and cabin fires to engine failures, fuel spills and evacuation incidents. Yet opportunities to practise these high-risk situations in realistic conditions are often limited. 

To help emergency crews build confidence and competence, Fire GO GmbH set out to develop a mobile training solution that could be deployed directly at airports worldwide. The goal was to create a realistic aircraft fire simulator capable of replicating a broad range of emergency situations while maintaining the highest safety standards for trainees and instructors alike.

The solution: mobile aircraft fire simulation system

Working alongside Mitsubishi Electric and Siebers Mechanical Engineering, Fire GO developed a mobile training platform based on Mitsubishi Electric's automation technologies. At the heart of the solution is the System-Q Control Platform, which manages all simulation processes across 28 fire points and ensures precise control of gas flow, safety functions and emergency shutdown procedures.

GOT Series HMI
terminals provide instructors with complete control over training scenarios, enabling real-time adjustments and monitoring throughout each exercise. At the same time, Mitsubishi Electric's visualisation and analytics solutions collect detailed data from sensors monitoring gas levels, temperatures and operational performance.

The result: safer training, better emergency readiness

he new solution enables firefighters to train on realistic aircraft emergency scenarios without leaving their airport environment. Thanks to the mobile design, advanced training can be delivered wherever it is needed, helping emergency teams build practical experience with the specific aircraft configurations they work with every day. 

Beyond realistic simulation, the platform also provides valuable performance insights. Detailed training data allows instructors to identify strengths, uncover areas for improvement and optimise training programmes based on objective results. Research cited in the project shows that simulation-based training can improve firefighter decision-making competency by 22%, highlighting the impact of realistic and repeatable exercises.

Why it matters?

In safety-critical environments, preparation is everything. This project demonstrates how industrial automation can support far more than manufacturing processes, helping emergency services develop the skills, confidence and readiness needed to respond effectively when lives are at stake. By combining realistic simulation with powerful control and analytics technologies, Mitsubishi Electric and Fire GO GmbH have created a solution that helps transform training into operational readiness.

Discover the solutions behind this case study

Have we sparked your interest? Contact us

0/255
Feltene merket med * er obligatoriske.

Our Stories

2025-11-18

NEWEnhancing firefighter safety: from simulation to life-saving decisions

Fire GO GmbH

ENDE
Se videoen på YouTube
#Data Collection/Analysis#Safety#Human-Machine Interfaces (HMIs) - GOT#Programmable Controllers MELSEC#MELSEC System Q