MITSUBISHI ELECTRIC Changes for the Better
Packaging

Sustainable packaging manufacturing

11.09.20263 min read

Packaging protects products, supports transport and enables manufacturers to prepare goods for storage and distribution. At the same time, packaging production involves materials, energy, machinery and multiple process stages. This makes packaging an important area for manufacturers looking to improve environmental performance. Sustainable packaging production focuses on how packaging is designed, formed, filled, sealed, labelled, handled and prepared for distribution. A more sustainable process does not depend on one technology or one material. It requires manufacturers to consider the complete packaging operation and identify where materials, energy and production resources can be used more effectively.

Why sustainable packaging production matters

Packaging production may involve several connected stages, including filling, forming, sealing, labelling, cutting, case packing and palletising. Each stage can influence the use of materials and energy, as well as the amount of product or packaging waste generated.

When these operations are not well coordinated, manufacturers may experience unnecessary interruptions, incorrect settings, rejected products or inefficient material flow. These issues can affect both production performance and environmental impact.

Sustainable packaging production aims to create more controlled and responsible processes. This may involve reducing avoidable waste, improving repeatability, using appropriate materials and managing equipment more efficiently.

The exact priorities depend on the application. A bottle filling line has different requirements from a pouch packaging machine or an end-of-line case-packing system.

For this reason, packaging industry sustainability should be considered at process level. The goal is not to make a general claim about sustainability, but to identify practical opportunities within a defined production environment.

Key principles of eco packaging manufacturing

Eco packaging manufacturing is based on the relationship between materials, equipment, energy and the final packaging format.

One important principle is material efficiency. The packaging needs to perform its intended function, but the process should also control how the material is fed, formed, filled, sealed or cut.

Another principle is process consistency. Incorrect positioning, poor sealing or inaccurate handling can lead to rejected products and wasted packaging material. More controlled machine operation may help manufacturers limit these avoidable losses.

Packaging manufacturers should also consider the complete production sequence. A change in one area can affect the rest of the line. For example, a different film or packaging format may require adjustments to forming, filling, sealing, cutting or product transfer.

Eco packaging manufacturing also requires clear measurement. Without data from the actual process, it is difficult to confirm whether a change has reduced material use, energy consumption or waste.

A responsible approach should therefore focus on defined production questions:

  • Where does material waste occur?
  • Which process stages require the most intervention?
  • Which machine settings affect the packaging result?
  • Where do interruptions or rejected products occur?
  • How can the process be monitored more effectively?

Sustainable materials used in modern packaging production

Sustainable packaging manufacturing can involve different materials and formats. The appropriate choice depends on the product, packaging requirements, transport conditions and the equipment used in the process.
The source materials describe applications involving bottles, labels, plastic film, pouches, sacks, cartons and cardboard cases.

Bottles may be used in filling applications where the product needs to be transferred into a solid container. The process requires coordination between the filling nozzle, container movement and flow control.
Plastic film is used in applications such as pillow packaging and vertical form-fill-seal systems. The film may need to be fed, formed, filled, sealed and cut in a controlled sequence.

Labels also form part of the packaging process. They may be applied to bottles or other cylindrical containers, and their positioning depends on the movement of the product and the accuracy of the labelling equipment.

Cardboard cases and cartons are used during secondary packaging and preparation for distribution. Case-packing systems need to handle products carefully while maintaining the required packaging sequence.

The use of a particular material should not be presented as sustainable without considering its complete application. The material, package design, production process, transport requirements and end-of-life conditions all influence the environmental result.

This is why sustainable packaging solutions need to be assessed in relation to the entire packaging system.

How green packaging factories reduce environmental impact

A green packaging factory focuses on controlling the production process and reducing avoidable environmental impact.
One area of attention is material waste. Forming, filling, sealing and cutting operations need to be coordinated so that packaging material is processed according to defined parameters.

Another area is product handling. Incorrect transfer, poor positioning or inaccurate filling can result in rejected products and additional material use. Control systems, sensors and coordinated equipment can support more repeatable operation.

End-of-line packaging also matters. Case packing, palletising and product transfer influence how finished goods are grouped and prepared for transport. When these stages are not coordinated with the rest of the line, they can create delays and additional handling.

A green packaging factory may also review how machines are started, stopped and adjusted. Clear sequences and accessible information can help operators identify operating conditions and respond to interruptions more effectively.

The result depends on the specific equipment and process. Automation alone does not make a factory sustainable. It can, however, provide a basis for more controlled operations and better measurement.

Manufacturers can review available packaging solutions when assessing how different packaging stages could be connected within one production environment.

The role of automation and digital technologies in sustainable packaging manufacturing

Automation and digital technologies can support sustainable packaging manufacturing by improving control, repeatability and process visibility.

A packaging line may include programmable controllers, sensors, drives, motion-control components and operator interfaces. Together, these technologies coordinate machine sequences and provide information about the operating conditions.
For example, a labelling system needs to coordinate product movement, label feeding and label positioning. A vertical form-fill-seal machine needs to control film movement, product dosing, forming, sealing and cutting.

When these activities are performed according to defined parameters, manufacturers may be better able to identify deviations and investigate sources of waste. However, any environmental benefit needs to be validated using data from the specific process.

Digital monitoring can also help operators understand machine status, active faults and production conditions. This information may support troubleshooting and reduce the time needed to locate a problem.
Automation may also be useful in end-of-line operations. Robotic or controlled systems can support case packing and palletising by following defined handling and stacking sequences.

The wider principle is similar to the one used in a smart automotive factory: connected automation can help manufacturers coordinate equipment and make production information more accessible.
Sustainability should remain the purpose of the improvement. Digital technology is useful when it helps answer a practical question about material use, energy, waste or process control.

Benefits of sustainable packaging production for businesses and consumers

Sustainable packaging production can provide several potential benefits, although the actual result depends on the application and implementation.

For manufacturers, better process control may help reduce avoidable waste and improve the repeatability of packaging operations. More structured production can also support troubleshooting and help identify where improvements are needed.
Controlled equipment operation may be relevant to filling, labelling, sealing and cutting processes. When the packaging line is coordinated, manufacturers can work with clearer operating sequences and more consistent product flow.

Sustainable packaging production may also support more responsible use of materials. This does not mean that one material is always better than another. The result depends on how the packaging performs during production, transport and use.

Consumers may benefit from packaging that performs its intended protective function while being designed with material use and end-of-life considerations in mind.

However, manufacturers should avoid making broad environmental claims without supporting evidence. Claims about reduced carbon footprint, lower waste or improved energy efficiency should be based on measurements from the relevant process.

Challenges in transitioning to eco packaging manufacturing

The transition to eco packaging manufacturing can involve technical, operational and material-related challenges.

A new packaging material may behave differently during forming, sealing, labelling or cutting. It may require different machine settings or changes to the packaging line.
Changes to the packaging format can also affect product handling and transport. A package that works well at one stage may create new requirements at another stage.

Existing equipment can create additional limitations. Older machines may use different control architectures or may not communicate easily with newer systems. Modernising one part of the line may therefore require careful planning.

Another challenge is the lack of reliable production data. Manufacturers cannot confirm the effect of a sustainability initiative without information about material use, rejects, interruptions and energy consumption.

There may also be a difference between a theoretical improvement and a practical one. A material may appear environmentally preferable, but its complete production and distribution requirements still need to be considered.

For these reasons, manufacturers should introduce changes in a controlled way and assess the results using defined criteria.

How to build a more sustainable packaging production process

A more sustainable packaging process should begin with an assessment of the current operation.

Manufacturers should examine the flow of products and materials through the line. This includes filling, forming, sealing, labelling, product transfer, case packing and palletising.

The next step is to identify where avoidable waste or inefficiency occurs. Relevant areas may include incorrect machine settings, rejected products, material damage, unnecessary handling or interruptions between process stages.
The equipment and control architecture should then be considered together. Sensors, controllers, drives, interfaces and communication systems all influence how the process is managed.

Manufacturers should also define how improvements will be measured. Depending on the application, this may include material consumption, rejected products, machine interruptions, energy use or changeover conditions.

Sustainability should be considered alongside product protection and production requirements. Packaging still needs to perform its intended function during filling, handling, storage and distribution.

The selected equipment should match the specific operation. For example, a horizontal packaging machine has different requirements from a bottle filling system, vertical form-fill-seal machine or palletising application.

A sustainable factory is not defined by one machine or one material. It is built through controlled processes, suitable equipment, measurable improvements and responsible production decisions.

FAQ section

What is sustainable packaging production?

Sustainable packaging production is the manufacture of packaging with greater attention to material use, energy consumption, waste, process control and the wider environmental impact of the packaging process.

What is eco packaging manufacturing?

Eco packaging manufacturing is an approach to producing packaging that considers the materials, equipment, production process, transport requirements and end-of-life conditions of the package.

How does a green packaging factory operate?

A green packaging factory uses controlled production processes, appropriate materials, efficient equipment and monitoring systems to reduce avoidable waste and manage resources more responsibly.

What materials are used in sustainable packaging manufacturing?

Materials may include bottles, plastic film, labels, pouches, sacks, cardboard and cartons. The suitability of each material depends on the product, packaging format, production process and distribution requirements.

What are the benefits of sustainable packaging production?

Potential benefits include better control of material use, reduced avoidable waste, more consistent production, improved process visibility and more responsible packaging decisions.

How can manufacturers reduce the environmental impact of packaging?

Manufacturers can review packaging formats, material flow, machine settings, rejected products, energy use and end-of-line operations. Improvements should be based on data from the specific production process.


Similar Articles


Topic

Packaging